Technical FAQs

Ask a Question

How long are the pegs supposed to be on the back side of LAL36300WB walking beam breaker?<br /><br />

The peg should be 0.35 inches long when the breaker is in the ``off`` position, and 1.30 inches long when the breaker is in the ``on`` position. Some adjustment can be done, by using pliers, hold the phenolic post and adjust the screw at end.




CTA-ID : 2028813
Was this helpful?
What can we do to improve the information ?