Technical FAQs

Ask a Question

What is the catalog number for a door mounted rotary handle for the Multi 9 breakers that will extend to the front door of my enclosure with the breaker mounted on the back surface of the enclosure?

Use an MG27046 operating subassembly and an MG27047 Door Interlock handle. From the front faceplate of the breaker to the door, the depth of the enclosure is 4.13`` minimum to 10.63`` maximum.

CTA-ID : 2029051
Was this helpful?
What can we do to improve the information ?