Technical FAQs

Ask a Question

Obsolete 24 Vdc power supply modules for Micrologic trip units: Catalog numbers, VA rating

Issue:
What are the catalog numbers and ratings of the OLD and OBSOLETE 24Vdc power supply modules for Micrologic trip units?

Product Line:
Circuit Breakers

Environment:
Applies to 24Vdc power supplies for Micrologic Trip Units supplied prior to 2005.

Cause:
Catalog numbers and ratings of the various types are required

Resolution:
Following are the catalog numbers and ratings of the 24Vdc power supplies sold prior to 2005 for Micrologic trip units.
Note that the catalog numbers are the same as the new ones.


 
Was this helpful?
What can we do to improve the information ?