Technical FAQs

Ask a Question

Is an ARP050, UL listed?

The ARP rating plugs are UL Listed under UL File # E10027, Volume 2, Section 20.


CTA-ID : 2029627
Was this helpful?
What can we do to improve the information ?