Technical FAQs

Ask a Question

Does the Powerpact P or R frame breaker with a 6.0A trip unit have phase-loss protection?

No it does not. A type ``P`` or ``H`` trip unit can use the undervoltage protection to detect loss of one phase, but it will not detect loss of multiple phases.


CTA-ID : 2029624
Was this helpful?
What can we do to improve the information ?