Technical FAQs

Ask a Question

Can the 8903L lighting contactor operate continuously with 277 VAC through the power contacts?

Yes, the device is rated 600 VAC maximum. However, the maximum rating for the device when connected with one pole to the load is 277vac when used for tungsten or ballast lighting

CTA-ID : 2029588
Was this helpful?
What can we do to improve the information ?