Technical FAQs

Ask a Question

What is the difference between utility meter sockets catalog number UTH7213B and UTH7213T?

The units are basically the same, except for the hub configuration on the top endwall. The UTH7213B has a hub opening in the top endwall that will accept a Type A hub (1`` through 2 1/2``). The UTH7213T has a hub opening in the top endwall that will accept a Type A-L hub (2`` through 4``).


CTA-ID : 2029574
Was this helpful?
What can we do to improve the information ?