Technical FAQs

Ask a Question

Can a QO200TR Air Conditioning Disconnect be used as a circuit breaker enclosure to mount a standard QO circuit breaker?

Issue:
Product Design

Product Line:
Enclosed Molded Case Switches

Environment:
Circuit breaker

Cause:
Application

Resolution:

No. The QO200TR is UL Listed and Labeled as an Enclosed Molded Case Switch and includes the QO200 Molded Case Switch.

Square D does offer a  catalog number QO2TR, which is UL Listed and Labeled as a circuit breaker enclosure and can be used to mount a 2-pole QO breaker, 60 ampere maximum.



 
Was this helpful?
What can we do to improve the information ?