Technical FAQs

Ask a Question

How is a RFK03L Class R Fuse Kit assembled to the switch fuse clips?

The RFK03L adapters barbed end is pushed firmly into a slot in the base near the LINE SIDE fuse clips. The circular portion of the adapter should engage the slot in the fuse clip. The adapter should not be able to be removed once properly installed. Three adapters are included in each kit.

CTA-ID : 2029686
Was this helpful?
What can we do to improve the information ?