Technical FAQs

Ask a Question

What is the thermal rating factor, and interrupting rating for a E-frame circuit breaker @ 400 Hz for the NF panel?

The thermal multiplier is .97 for all E frame amperages. The interrupting rating is 1/10 of the 60Hz interrupting rating.

CTA-ID : 2029607
Was this helpful?
What can we do to improve the information ?