Technical FAQs

Ask a Question

What is the purpose of the 9080 GH52 fanning strip shown on digest 172 page 22-5?<br /><br /><br /><br />

The fanning strips are used to build a detachable wiring harness. They are separate units that snap together to make a harness of any size..


CTA-ID : 2029581
Was this helpful?
What can we do to improve the information ?