Technical FAQs

Ask a Question

Can a 9013FSG2J20 pressure switch be installed horizontally, rather than the standard vertical mounting?

Yes. This unit can be mounted horizontally and still work properly.


CTA-ID : 2029522
Was this helpful?
What can we do to improve the information ?