Technical FAQs

Ask a Question

What ground kit is used with HU366 safety switch?

The Ground Kit for the HU366 is PKOGTA2. The ground kit consists of two lugs, with wire range of #2 - #2/0 AWG. Two kits are required if the grounding conductors are run in parallel.


CTA-ID : 2029467
Was this helpful?
What can we do to improve the information ?