Technical FAQs

Ask a Question

Is there a comb busbar or multiple input connection device available for QOU type breakers?

No. At this time, there are no comb busbars or similar multiple input connection devices available for QOU breakers.

CTA-ID : 2028918
Was this helpful?
What can we do to improve the information ?