Technical FAQs

Ask a Question

Do the Integral Starters provide low voltage protection?

These devices are electrically held in nature. Therefore when the control scheme uses momentary signals in conjunction with a holding circuit contact low voltage protection will be present. On the other hand, if maintained controls are supplied then low voltage protection is not present.

CTA-ID : 2028991
Was this helpful?
What can we do to improve the information ?