Technical FAQs

Ask a Question

What is the part number for the ``wing nut plug`` used to seal the hole in the joint cover on outdoor feeder (NEMA 3R) bus duct 800A to 5000A?

It is 45118-041-01. The wing nut plug is used ONLY on vertical risers and edgewise horizontal run applications. It should not be used on flatwise horizontal runs. Refer to the installation instructions - part number 45123-921-01.


CTA-ID : 2029459
Was this helpful?
What can we do to improve the information ?