Technical FAQs

Ask a Question

Can the HOM612L100F/S, HOM48L125GC, HOM612L100RB and HOM48L125GRB, Fixed main lugs load centers, be converted to a main breaker load center?

Issue:
product features

Product Line;
Homeline load centers

Environment;
Convert to main breaker

Cause:
Application

Resolution;
ALL these load centers are Fixed Main Lug and are not convertible to a main breaker.

The only option to convert these panels to a main breaker load center would be to Back Feed a HOM, 2-pole branch breaker as the main. This would require a 2pole Homeline branch breaker rated less than the mains maximum rating or what is marked on the wiring diagram of the load center and it would require the retaining kit catalog number HOM1RK. The Back-Fed option will use 2 of the load centers 4 or 6 spaces, depending on the catalog number.




 
Was this helpful?
What can we do to improve the information ?