Technical FAQs

Ask a Question

Can the HOM24L70F, Fixed main lugs load center, be converted to a main breaker load center?

Issue:
product features

Product Line;
Homeline load centers

Environment;
Convert to main breaker

Cause:
Application

Resolution;
This device is a Fixed Main Lug and it CANNOT be converted to a main breaker load center.

 
Was this helpful?
What can we do to improve the information ?