Technical FAQs

Ask a Question

Can a Model 6 LVMCC section be added and the cross bus connected to either side of an existing section provided room is not an issue .

Yes , if the 2 sections have the same size and type of bus


CTA-ID : 2029021
Was this helpful?
What can we do to improve the information ?