Technical FAQs

Ask a Question

Does HVL/cc switchgear with auto transfer require a 20`` wide empty section to mount the controls?

Yes. The product configurator will not add this section automatically, but it is needed since the low voltage compartments are very small for HVL/cc. This section can be located between the mains or near them.

CTA-ID : 2029668
Was this helpful?
What can we do to improve the information ?