Technical FAQs

Ask a Question

What is the catalog number for the handle padlock attachment for a QO(B)AS or EH(B)AS Powerlink Breakers?

QOAS-PA is the handle padlock attachment for the QO(B)AS Powerlink Breaker and EHAS-PA is the handle padlock attacment for the EH(B)AS Powerlink Breaker.


CTA-ID : 2028537
Was this helpful?
What can we do to improve the information ?