Technical FAQs

Ask a Question

Is there an optional neutral lug or ground bar lug for a HOMELINE load center that will accept a larger wire than the standard neutral bar or ground bar will accept?


Product Line:
HOMELINE Load Center


Yes, there are optional, field installed neutral lugs that can be installed on most HOMELINE load centers. They could also be installed on an equipment ground bar. The options include: LK70AN (#12-2 Al or #14-4 Cu), LK100AN (#6-2/0 Al/Cu), LK125AN (#14-2/0 Al/Cu), LK150AN (#2-3/0 Al/CU) or LK225AN (#4-300 kcmil Al/CU).

CTA-ID : 2028509
Was this helpful?
What can we do to improve the information ?