Technical FAQs

Ask a Question

Which parts of a stainless steel NQOD panel enclosure are actually constructed of stainless steel?

The box and door are both constructed of stainless steel. The interior deadfront standard steel rawstock painted ANSI 61 gray.


CTA-ID : 2028503
Was this helpful?
What can we do to improve the information ?