Technical FAQs

Ask a Question

Is the Frequency Reference for keypad command with the ATV58 retained on loss of power?

On loss of power the local speed reference (Frh or LFr) goes back to the Low Speed setting (LSP).
The last reference will be lost.


CTA-ID : 6827
Was this helpful?
What can we do to improve the information ?