Technical FAQs

Ask a Question

What could prevent menu 8 from showing parameters P001 through P005 for entering the IP address?

If keypad version is 3.0 or earlier you cannot program this card.
The keypad must be later than 3.0 for the parameters for the Ethernet card to be displayed.



CTA-ID : 2008787
Was this helpful?
What can we do to improve the information ?