Technical FAQs

Ask a Question

What are the ampere rating frame sizes and ampere rating ranges for EZM Main Fusible Switches?

Issue:
Selection

Product Line:
EZM

Cause:
Selection Criteria

Resolution:
EZ METER-PAK Main Fusible Switches accept only Class T (300 VAC) fuses in the following frame sizes where each fuse is available in a select range of ampere ratings (order fuses separately). Note: Fuse Reducers are not acceptable for use in EZM main fusible switches.
400A Frame Class T (300VAC maximum) Fuses range form 225A minimum to 400A maximum.
600A Frame Class T (300VAC maximum) Fuses range form 450A minimum to 600A maximum.
800A Frame Class T (300VAC maximum) Fuses range form 601A minimum to 800A maximum.
1200A Frame (Available in Single Phase Only) Class T (300VAC maximum) Fuses range form 801A minimum to 1200A maximum.



CTA-ID : 2028238
Was this helpful?
What can we do to improve the information ?