Technical FAQs

Ask a Question

Is the SC3040M200F supplied with a factory installed bypass on the meter socket?

Issue:
Product design

Product Line:
Combination Service Entrance Device

Environment:
Meter socket bypass

Cause:
Application

Resolution:
No, a bypass is NOT supplied with the SC3040M200F and a Field installable bypass is not available for this device.


CTA-ID : 2028401
Was this helpful?
What can we do to improve the information ?