Technical FAQs

Ask a Question

Is a bypass supplied on the SU3040D400FB Combination Service Entrance Device?

Yes, a manual link bypass is supplied factory installed on this device. The manual link bypass provides the same bypass function as a test block bypass.


CTA-ID : 2028367
Was this helpful?
What can we do to improve the information ?