Technical FAQs

Ask a Question

What is required to convert the Homeline, Convertible Main breaker load centers that uses a QOM2 frame size(for example: HOM3040M200TC) to a Main Lug Load Center?

Issue:
Product design features

Product Line:
Homeline load centers

Environment;
Conversion to main lug

Cause:
Application

Resolution:
The Homeline Convertible Main breaker load centers that uses a QOM2 Frame size, can be converted to a Main lug load center by removing the QOM2, Main Breaker and obtaining the Main Lug kit, part number QOL225 and possibly the QOM2FP Main Breaker opening Filler Plate. The filler plate would be required when the Main Breaker knockout has been removed from the deadfront trim.



CTA-ID : 2028451
Was this helpful?
What can we do to improve the information ?