Technical FAQs

Ask a Question

What wire size does the S33930 subfeed lug kit accept?

Issue:
What wire size does the S33930 subfeed lug kit accept?

Product Line:
I-Line panelboards and accessories sold and supported in the USA.

Environment:
Application

Cause:
Selection

Resolution:
It accepts (4) #3/0 AWG - 600 kcmil and takes up 15" of mounting height in the panelboard.  It will only install into an HCP, HCRU or HCP-SU panelboard 


 
Was this helpful?
What can we do to improve the information ?