Technical FAQs

Ask a Question

In the I-Line II End Cable Tap Boxes, are different lugs available other than the standard 600kcmil?<br /><br />

Yes, lugs such as 750 kcmil are available but must be specified at the time of order.

CTA-ID : 2028436
Was this helpful?
What can we do to improve the information ?