Technical FAQs

Ask a Question

What is the difference between Class 9036 & 9037 devices?<br />

The 9036 is an open tank device. The 9037 is a closed tank device.


CTA-ID : 2028300
Was this helpful?
What can we do to improve the information ?