Technical FAQs

Ask a Question

What is the Short Circuit Current Rating (SCCR) for the SC816F200S Combination Service Entrance Device?

Issue:
Application

Product Line:
CSED

Cause:
Clarifying short circuit current rating

Resolution:
The SCCR for this device is 22,000 RMS Symmetrical Amperes at 120/240Vac maximum. Standard 10,000 AIC HOM and HOMT branch breakers are series rated with the QOM2-VH main breaker.


CTA-ID : 2028230
Was this helpful?
What can we do to improve the information ?