Technical FAQs

Ask a Question

How many operating cycles can the class 9012 operate in a minute ?<br /><br />.

Operating speeds up to 200 cycles power minute are not detrimental to the life of the diaphram.


CTA-ID : 2028156
Was this helpful?
What can we do to improve the information ?