Technical FAQs

Ask a Question

What is the terminal lug data for a QC2442M200CH Combination Service Entrance Device?

The main phase and neutral lugs accept a #6 AWG - 350 KCMIL copper or aluminum conductor. The service ground lug accepts a #8 - #2/0 AWG copper or aluminum conductor.


CTA-ID : 2028123
Was this helpful?
What can we do to improve the information ?