Technical FAQs

Ask a Question

What is the terminal data for the NEMA size 6 contactors and starters?

Power terminals will accept one or two #250 to #500 kcmil copper conductors per phase. Control terminals will accept one or two #16 - #12 AWG copper conductors per terminal.


CTA-ID : 2013725
Was this helpful?
What can we do to improve the information ?