Technical FAQs

Ask a Question

What UL File number are Combination Service Entrance Device listed under?

Issue:
Product UL listing

Product Line:
 Combination Service Entrance Devices

Environment:
UL File Number

Cause:
Application Request

Resolution:
All the Combination Service Entrance Devices (CSEDs) are listed in the UL File #E6294.


CTA-ID : 2028125
Was this helpful?
What can we do to improve the information ?