Technical FAQs

Ask a Question

What is the terminal lug data for the SC3040M200F Combination Service Entrance Device?

Issue:
Lug data

Product Line:
Combination Service Entrance Devices

Environment:
Main lugs

Cause:
Wire sizes

Resolution:
The main phase and neutral lugs accept a (1) #4 AWG - 250 KCMIL copper or aluminum conductor. The service ground lug accepts a (1) #14 - #2/0 AWG copper or a (1) #12 - #2/0 AWG aluminum conductor.


CTA-ID : 2028096
Was this helpful?
What can we do to improve the information ?