Technical FAQs

Ask a Question

What is the terminal lug data for a QC816F150C Combination Service Entrance Device?

The main phase and neutral lugs accept a #6 AWG - 350 KCMIL copper or aluminum conductor. The main service ground lug accepts a #12 AWG - #2/0 AWG aluminum or a #14 AWG - #2/0 AWG copper conductor.


CTA-ID : 2028074
Was this helpful?
What can we do to improve the information ?