Technical FAQs

Ask a Question

What is the terminal lug data for a SC816F200S Combination Service Entrance Device?

The main phase and neutral lugs accept a #4 AWG - 250 KCMIL copper or aluminum conductor. The service ground lug accepts a #14 - #2/0 AWG copper or a #12 - #2/0 AWG aluminum conductor.

CTA-ID : 2028056
Was this helpful?
What can we do to improve the information ?