Technical FAQs

Ask a Question

Can a HOMRBGK2 Generator Interlock Kit be used with a HOM816M200FTRB?

ISSUE:
Selecting a generator interlock kit for a Homeline load center.

PRODUCT LINE:
Homeline Load Centers

ENVIRONMENT:
Current Series Homeline Load Centers.

CAUSE
:
New Series for this particualr catalog number.

RESOLUTION
Yes, if the HOM816M200FTRB is a Series S02 or S03. If the HOM816M200FTRB is a Series S01, use the HOMCGK2 Generator Interlock Kit. (revised the FAQ to include Series S03)



CTA-ID : 2028103
Was this helpful?
What can we do to improve the information ?