Technical FAQs

Ask a Question

What is the terminal lug data for a SC8L125S Combination Service Entrance Device?

Issue:
Product Main Lug Wire size

Product Line:   
Combination Service Entrance Device

Environment:   
Line Terminal Sizes

Cause:  
Installation of appropriate wire sizes for the Main lugs

Resolution:  
The main phase, neutral and service ground lugs accept a (1) #6 AWG - 2/0 AWG copper or aluminum conductor.


CTA-ID : 2028048
Was this helpful?
What can we do to improve the information ?