Technical FAQs

Ask a Question

What is the terminal lug data for a SC2040M200C Combination Service Entrance Device?

Issue:
Product Feature

Product Line:
CSED

Cause:
Clarifying lug wire range

Resolution:
The main phase and neutral lugs accept a #6 AWG - 300 KCMIL copper or aluminum conductor. The service ground lug accepts a #14 - #1/0 AWG copper or a #12 - #1/0 AWG aluminum conductor.


CTA-ID : 2028112
Was this helpful?
What can we do to improve the information ?