Technical FAQs

Ask a Question

Are the feed through lugs de-energized(or power turned OFF) when the main breaker in HOM816M200FTRB is turned to the OFF position?

Issue:
Product Design Feature

Product Line:
Homeline load centers

Cause:
Operation and/or application

Resolution:
Yes, the main breaker controls the power (or current flow) to the internal bus bars (or branch breaker bus bars) and the feed-through lugs are located at the bottom of the bus bars.

 
Was this helpful?
What can we do to improve the information ?