Technical FAQs

Ask a Question

What is the difference between the PK23GTA and the PK23GTAL ground bar?

Issue:
Product Features

Product Line:
Load Center Accessory

Cause:
Clarifying product features differences

Resolution:
Both ground bars have 23 terminals for (1) #14-#4 or (2) #14-#12 CU wire or (1) #12-#4 or (2) #12 or #10 AL wire. The PK23GTAL has an additional terminal for (1) #1-4/0 CU or AL wire.


CTA-ID : 2028100
Was this helpful?
What can we do to improve the information ?