Technical FAQs

Ask a Question

What is the Short Circuit Current Rating (SCCR) for the RC2040M200C Combination Service Entrance Device?

The SCCR for this device is 22,000 RMS Symmetrical Amperes at 120/240Vac maximum. Standard 10,000 AIC HOM and HOMT branch breakers are series rated with the QOM2-VH main breaker.

CTA-ID : 2028209
Was this helpful?
What can we do to improve the information ?