Technical FAQs

Ask a Question

What does the S247 suffix on an ATV66 part number indicate?

This suffix indicates that the drive has special firmware to provide brake sequence parameters to be used for hoisting applications. This special firmware was available in Europe but was not commercialized in the United States.


CTA-ID : 2028105
Was this helpful?
What can we do to improve the information ?