Technical FAQs

Ask a Question

Can a Double Throw Safety Switch be mounted directly to ACQ (Alkaline Copper Quaternary) Pressure-Treated wood?

Issue:
Product Design Feature

Product Line:
Double throw safety switches

Environment:
Switch mounting

Cause:
Mounting to treated wood

Resolution:
The chemical compounds used in ACQ preserved wood products may have an adverse effect on the metal enclosure and the fasteners used to secure the enclosure to the wood surface. It is not recommended to mount the enclosure directly to the ACQ preserved wood. Spacer materials or other physical barriers are recommended to prevent direct contact of the ACQ preserved wood to the enclosure. Fastener specifications recommended for direct contact to the ACQ preserved wood are available on the Universal Forest Products website. A link to their website pages concerning the safe handling, use and fasteners has been provided below.
https://www.ufpi.com


CTA-ID : 2028454
Was this helpful?
What can we do to improve the information ?