Technical FAQs

Ask a Question

What is the function of a bypass, when one is supplied, on a Combination Service Entrance Device?

Issue:
Product Function

Product Line:
CSED

Cause:
Product Function

Resolution:
A meter socket supplied with a bypass can provide continued service, by manual operation of the bypass, when the watt-hour meter has been removed. A bypass is only for temporary duty service and should only be engaged by utility company personnel.


CTA-ID : 2028131
Was this helpful?
What can we do to improve the information ?