Technical FAQs

Ask a Question

What is the part number for 60 amp fuse clips for the D10S2 or D10S2H disconnect switch?

Select from below based on application requirements:

250 volt, Class H & K = D12D22
250 volt, Class R = D12DR22
600 volt, Class H & K = D12D62
600 volt, Class R = D12DR62
600 volt, Class J = D12DJ2



CTA-ID : 2028032
Was this helpful?
What can we do to improve the information ?